NumericFunctions.Absolute value expression

Returns the absolute value of a numeric expression

Format

ANSI-SQL Format:

ABS( Expr )

ODBC Format:

{{ FN ABS( Expr ) }}

Remarks

Returns the absolute value of Expr, which is always zero or a positive number. Expr can be any expression, if it is not numeric then zero is returned.

Example:

ABS( 7 )

{FN ABS( -7 )}


Disclaimer

ClearSCADA 2017 R3